4/28/2011 11:54 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1165) |
Dear Corb, Perhaps this link might help: What should you watch out for when configuring a CP342-5 as DP master? Look at point 5. Best regards, Wizard |
4/29/2011 11:00 AM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating: (1053)
|
Definetely NOdear Corb (FDL is for PLC-PLC communication, you are doing Profibus DP communication). May I suggest that you have anothercareful read ofthelink that Wizardprovided you withand also check the following two links: CP 342-5 -- How do you program data communications when your DP slave only has outputs?(I presume this the case as you have not mentioned any DP_RECV calls?). Which version of the function blocks do you need to operate a CP 342-5? I hope this helps (if it doesn't, please upload your S7 project here for evaluation). |
Cheers |
|
Follow us on