5/24/2011 11:07 AM | |
Joined: 10/22/2008 Last visit: 7/5/2024 Posts: 368 Rating: (5) |
Thats exactely how I thught. However could you explaint it to me how to set ip adress of the IM 151-3? |
5/24/2011 11:34 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello, You can use Primary Setup Tool: Primary Setup Tool (PST) Version V3.2 and New Version V4.0 for Address Setting of SIMATIC NET Industrial Ethernet Products Available for Downloading Or in STEP 7 go to PLC-> Edit Ethernet Node Best regards, Wizard |
5/24/2011 11:48 AM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating: (1053)
|
Hello Oscar_83PL there seems to be some confusion going on here in this thread so allow me to go back to basics: You have the following hardware: S7 313 CPU CP 343-1 LEAN A bunch ofIM151-3based Profinet I/O stations You want to: Link the IM151-3based Profinet I/O stations to the S7 CPU via the CP343-1 LEAN Have I understood you correctly thus far? If so, the simple answer is that it is NOT possible. Wizard's previous advise is correct, the CP343-1 LEAN can NOT be a Profinet I/O Controller (it can only be a Profinet I/O device which is akin to beingDP Slave in Profibus). Have a look too at the link belowfor more on this: What differences exist in the 300-series Industrial Ethernet CPs? Solution: Upgrade the CPU to a PN one or buy a CP343-1 that can be used as a Profinet I/O Controller Once you made that choice you'll find all the relevant info on how to set it all up in the links below: PROFINET IO - Configuration & Diagnostics Where can you find information on the topic of PROFINET? I hope this helps |
Last edited by: fritz at: 5/24/2011 11:50 AMCheers |
|
This contribution was helpful to1 thankful Users |
5/25/2011 1:18 PM | |
Joined: 10/22/2008 Last visit: 7/5/2024 Posts: 368 Rating: (5) |
I think it would be easier to change im351-3 to im351-8 (PN with own CPU). |
Follow us on