9/14/2011 12:52 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
If you didn't install Update 1 for SP1 of TIA11 - try it. Updates for STEP 7 V11 SP1 and WinCC V11 SP1 Under what OS did you install TIA Portal. Make sure your OS is compatible with TIA. Best regards, Hristo MIhalev |
9/14/2011 3:02 PM | |
Posts: 41 Rating: (3) |
Okay. I installed the update whichUMENCHOsuggested and the problem persists. If not worse. The maximize, shrink problem still occurs. What is happened more frequently is if I press F1 then the help appears, but nothing loaded in the screen and then closes again. If I try again it will sometimes remain open. Once it is open, if I minimize the help and carry on working then if I click on just about anything else then I get the "application has encountered an error and needs to restart" error. |
9/14/2011 3:03 PM | |
Posts: 41 Rating: (3) |
I see an update 2 has just appeared! |
9/14/2011 3:31 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Aaa really it is there. Did you try it already? Best regards, Hristo Mihalev |
9/14/2011 3:34 PM | |
Posts: 41 Rating: (3) |
Still downloading at the moment. Internet very very slow :( |
Follow us on