11/11/2011 9:42 AM | |
Joined: 1/26/2007 Last visit: 5/2/2024 Posts: 123 Rating: (4) |
Hello i know to configure the area pointers , but still i have some thing regardings the alarm message that i do not understand correct . i take-it out one plc , but i do not know haw to take out the the message, to have the correct order inside , and to get the correct event . now i keep the plc configured insidet OP 37 to not have malfunction to OP . from area pointers i see for ex the event message for Extr1 from 1 to 96 , but in the list i have earlier the Extr2 in list instead of starting from 97 . I understood rong the nr from 1 to 96 fro area pointers->event message EXTR1 1-96 where is assignet the linte message to the correct M from PLC (duw to we run to MW inside the evvent pointers .. not with DB ). Can somebody help me with some clues Please See the pictures to better understand AttachmentOP37 event message.zip (126 Downloads) |
Follow us on