6/5/2011 5:00 PM | |
Joined: 1/28/2009 Last visit: 6/11/2024 Posts: 6841 Rating: (1360) |
For members who are interested in implementing complex loop configuration with PID controllers, There are series of examples provided by SIEMENS in Modular PID Control Package. The function implemented by using blocks in ModPID library of Modular PID Control and the samples are embedded in zEN28_4_ModCon.They are 12 and named from EXAMPLE01 to EXAMPLE12.Discription of Check this manual for more information: Section 2-Description of the Functions Section 3-Examples List of some examples: Example 5: Multiple-Loop Ratio Controller Example 6: Blending Controller Example 7: Cascade Controller Example 9: Controller with Feedforward Control (CTR_C_FF) Example 10: Range Splitting Controller (SPLITCTR) Example 11: Override Controller (OVR_CTR) Example 12: Multiple Variable Controller regards AttachmentMPD.zip (1034 Downloads) |
This contribution was helpful to3 thankful Users |
6/7/2011 1:14 AM | |
Posts: 510 Rating: (117) |
I put this together a few years ago to compare and contrast the various PID offerings for Step 7. Even though there have been updates to the packages, the basic information should still be applicable. billwest
AttachmentPID.pdf (1085 Downloads) |
This contribution was helpful to2 thankful Users |
6/1/2012 4:22 PM | |
Posts: 5 Rating: (0) |
we dont have that sample project inside our pc...where can i get that file...??i've search for it but there's no file for that sample... |
Follow us on