8/28/2012 11:40 AM | |
Posts: 739 Rating: (55)
|
With DriveMonitor (or STARTER)only one dirve can be controlled. With AOP up to 31 In Master mode the AOP can control up to 31 inverters connected in a multi-drop arrangement. Full operator control of each inverter is possible with access to all normal inverter and AOP internal parameters. Control of the inverters may be individual or by the broadcast method previously described. In the broadcast mode it is possible only to start and stop the motor directly simultaneously. With AOP and external power supply ~ 25m cable should be possible http://support.automation.siemens.com/WW/view/de/10447716 http://support.automation.siemens.com/WW/view/en/24532563 http://support.automation.siemens.com/WW/view/en/17524693 http://support.automation.siemens.com/WW/view/en/17524482 |
Follow us on