10/25/2012 1:40 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello Milosh, Have a look at the following links: Which organization blocks do youhave to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? Enabling a disabled DP slave with SFC 12 "D_ACT_DP" And have a look at online help of STEP 7, search for "Report System Error" (RSE) Best regards, Wizard |
10/25/2012 1:58 PM | |
Joined: 8/16/2010 Last visit: 5/16/2024 Posts: 636 Rating:
|
OK... I think that OB82 is good enough. But what code do I need to check which module is fault? |
10/25/2012 2:17 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Perhaps this link might help: PROFINET IO - Diagnostics Processing in the User Program link to manual: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 Best regards, Wizard |
10/25/2012 2:37 PM | |
Joined: 8/16/2010 Last visit: 5/16/2024 Posts: 636 Rating:
|
OK... Thanks a lot! |
Follow us on