11/22/2012 9:45 AM | |
Posts: 112 Rating: (2) |
dear sir any manual or steps to configure the web navigator (procedure to setup the connection) |
11/22/2012 10:58 AM | |
Joined: 8/31/2010 Last visit: 10/8/2024 Posts: 1522 Rating: (228) |
Hello GOWDA, Refer Chapter 9.16.4 from the WinCC Professional v11 SP2 - System Manual Online Version - Web Navigator |
Like it? Rate it! |
|
11/22/2012 11:08 AM | |
Posts: 112 Rating: (2) |
dear sir, so we required wincc professional v11.0 sp2 is required for web navigation or it is possible in sp1 |
11/22/2012 1:41 PM | |
Posts: 3037 Rating: (192)
|
Hello GOWDA, You should use WINCC V11 SP2 if you use the option web navigator. Tweety |
11/22/2012 1:57 PM | |
Joined: 8/31/2010 Last visit: 10/8/2024 Posts: 1522 Rating: (228) |
Hello GOWDA, of course it works with SP1 also. But it is always recommended to work with latest software, as SP2 is available for download in internet (at no cost) |
Like it? Rate it! |
|
11/26/2012 4:55 AM | |
Posts: 112 Rating: (2) |
dear ganes thanks for supporting ............................... |
Follow us on