1/6/2015 6:43 PM | |
Joined: 10/15/2014 Last visit: 10/29/2023 Posts: 80 Rating: (2) |
thanks for the reply WWEE. i think i read that there was a limit of 9 TDE's linked together, is that the case?
|
1/6/2015 8:03 PM | |
Posts: 15 Rating: (0) |
Hi WWEE It's possible to connect 2 logo8 with TDE (have 2 ports), without CSM, make a separate program for each logo and using network inputs and outputs, if possible ¿as they have to configure the logo and the TDE? |
Follow us on