3/15/2015 5:49 PM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating:
|
i have the problem with the Y-link IM module which remains in SF (continues) and bf 2 blinking and my y-link is now physically connected to the Sipart but i have configured it on the my hardware configuration so as to fulfill the master/slave requirement ....... so is there any way to hide this LED on the module including all this my CPU(s7-412-5h) does not shows any bus or system fault ? will i have to remove the y-link from the hardware config so as to remove this fault? answer is awaited.......... ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/16/2015 3:24:15 PMNew subject after splitting Thanks and Regards |
|
Follow us on