3/19/2015 8:18 PM | |
Joined: 11/4/2009 Last visit: 10/3/2024 Posts: 6 Rating: (0) |
Hi everyone, I have just come across an issue with changing my pg/pc interface. I have a softing netlink pro eth and installed the software for it and used it previously. When i go to select the interface i can only select items in the list and the netlink is missing. Also i cannot add another interface as the select button is greyed out. In the list of interfaces there are 3 showing active. I have uninstalled step 7, simatic NET and wincc flex. I did not uninstall wincc 7.2. Installing step 7 again still shows the same screen. Can anyone help with this?? AttachmentPGPC error.docx (131 Downloads) |
Follow us on