7/16/2015 2:44 PM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Hi All, 1. Give some technical document for remote monitoring (Example: Wind Mill Data) Thanks |
7/18/2015 7:52 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, There is a link grouping sveral further links regarding remote communcation and control: There are two major categories of remote control applications: If you think about using a small PLC like an S7-1200, |
Best regards |
|
7/18/2015 7:56 PM | |
Joined: 5/9/2011 Last visit: 9/11/2024 Posts: 71 Rating: (5) |
How about using Teamviewer for remote monitoring. Here is also a previous post on how to use Teamviewer VPN. Also another post about wireless communication here. I am also attaching the pdf for the Teamviewer VPN set-up. If it is only for monitoring purposes maybe you are looking for a SCADA system that can use cloud server to connect to your PLC? AttachmentHow%20to%20setup%20Teamviewer%20VPN.pdf (67 Downloads) |
Last edited by: Bosbreker at: 7/18/2015 7:59:51 PM |
|
Follow us on