2/8/2008 6:19 PM | |
Posts: 2661 Rating: (279) |
What is your PG/PC interface set to? |
2/11/2008 8:35 AM | |
Posts: 14 Rating: (0) |
No, it doesn't work! |
2/11/2008 11:21 AM | |
Posts: 4 Rating: (0) |
PLCSIM 5.4 support Ethernet connections Until now, S7-PLCSIM used a standard connection via MPI to address 2. With S7-PLCSIM V5.4 you can search through the STEP 7 projects and select a networking subscriber for the establishment of a simulation connection. S7-PLCSIM will simulate the CPU of the selected subscriber, all the subscribers belonging to the CPU and the subnetwork of the selected subscriber.
|
Follow us on