5/30/2016 10:03 AM |
|
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (942) |
Hello dmelliot, I played with your code. I think you have to change your code to the following:
Can you try and report back. I have no error codes |
If I could help you, you can use the RATE button. Thank you. |
|
5/31/2016 9:31 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (942) |
Hi, During compiling of the SCL source, the data block is not known, so the SCL compiler cannot find the corresponding data type by means of the symbol table and tag declaration of the DB in question. If the DB is now accessed by absolute addresses, S7-SCL assumes that the data type is BOOL, BYTE, WORD or DWORD. |
If I could help you, you can use the RATE button. Thank you. |
|
6/1/2016 9:10 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (942) |
Here is some official documentation: You can use DB120.DBW[AP] section of your code, but you cannot link this to the variable: "DEV". But, on this section this is all I know |
If I could help you, you can use the RATE button. Thank you. |
|
6/7/2016 10:05 AM | |
Joined: 8/21/2014 Last visit: 10/8/2024 Posts: 1024 Rating: (14) |
New question published by ivan-2 is split to a separate thread with the subject Script not working. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on