6/21/2016 2:46 PM | |
Posts: 67 Rating:
|
Dears, I have PLC-1214 with one DI module, how to read the LED status (normal or error) for both devices using OB82 .. or anyway ?? Regards, |
6/21/2016 5:03 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello AZRAIQI, I have found this i don't know if you already read perhaps might help you: How do you proceed when peripheral device errors are detected by ... |
This contribution was helpful to
3 thankful Users |
6/21/2016 7:13 PM | |
Posts: 439 Rating:
|
Hello Ste39, I tried to do it with a DI DQ 6ES7 223-1BH30-0XB0, but I miss something when it is time to enable the diagnostic of the module. I can't find a place to enable the diagnostic in the property of the module. If I try to do the same thing with an analog input module, it is as describe in the FAQ you gave. For what I understand of the FAQ, the use of this for the signal module is to detect a missing encoder or the lost of load power. Thanks for the information. Best regards, Hugo |
This contribution was helpful to
1 thankful Users |
6/21/2016 8:01 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Hugo, On the bottom of the FAQ is a link for "compatible" modules, I think the diagnostic is not possible with all modules Additional Information More information about diagnostics-compatibleanalog signal modules (SM) and signal boards (SB)is available in the SIMATIC S7-1200 Automation System manual (Entry ID:36932465).
|
Last edited by: Ste39 at: 6/21/2016 8:03:15 PMAdditional info in English |
|
This contribution was helpful to
1 thankful Users |
6/22/2016 1:01 PM | |
Posts: 67 Rating:
|
I try to use OB82 as the photo attached and it's working fine, also i used the LED function (it's seem work only with the LED for the CPU) thanks all Regards, Attachmentdiag.zip (335 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on