9/10/2016 12:05 PM | |
Joined: 1/21/2016 Last visit: 4/22/2023 Posts: 83 Rating: (1) |
what is steps to troubleshoot cpu 317 2pn/dp |
Amr Ali |
|
9/10/2016 2:58 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello amrelhajali; At what level do you need to troubleshoot, configuration, hardware, programming? Step 7 has an excellent tool to help diagnose problems on the PLC, the diagnostic buffer, which collects messages from the CPU on events that affect it. Of course diagnostic LEDs are also available to help understand problems on the CPU and I/O modules. You will find a basic document on diagnostics in the manual Programming with Step 7, you can use it for a first step; I have printed the section on diagnostics in pdf format, you will find it in attachment. If this is much too general for you, or if you have more specific questions don't hesitate to come back to the forum. Hope this helps, Daniel Chartier AttachmentStep7_5_5_diagnostics.pdf (53 Downloads) |
This contribution was helpful to1 thankful Users |
9/11/2016 10:03 AM | |
Joined: 1/21/2016 Last visit: 4/22/2023 Posts: 83 Rating: (1) |
thanks the manual was very helpful :) |
Amr Ali |
|
This contribution was helpful to1 thankful Users |
Follow us on