10/10/2016 3:42 PM | |
Joined: 3/14/2016 Last visit: 8/11/2023 Posts: 162 Rating: (45) |
Hi, what was the error value read? For measurements between 1-5V and 0-20 or 4-20mA, here are the possible values for analog modules: What is the configuration of the module? Go to the PLC Device Configuration and right click on the Module under Proprieties/Configuration. Maybe it can be filtering or settings. I'll attach the PDF for Analog Modules. AttachmentAnalog Module.pdf (106 Downloads) |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
10/11/2016 9:07 AM | |
Joined: 11/1/2007 Last visit: 8/8/2024 Posts: 14 Rating: (0) |
Hi kijo Have a look at this faq |
Joakim Waldau |
|
This contribution was helpful to1 thankful Users |
Follow us on