1/18/2017 9:03 AM | |
Joined: 2/10/2015 Last visit: 6/18/2024 Posts: 14 Rating: (0) |
Hi How do convert TAK,BEC,XOD,INC STL code to LAD? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/18/2017 1:54:17 PMNew subject after splitting |
|
1/18/2017 12:32 PM | |
Joined: 3/14/2016 Last visit: 9/1/2024 Posts: 162 Rating: (45) |
Hi William, I have already tried discussing this subject on other topics (Dynamic function block call in SCL) but we agreed that it is something that is not implemented yet on the 1200 processor architecture. A feature that I was expecting on 1200 have already come with the V14, the Create and Delete DB instructions. I couldn't simulate this functions though because there are a few issues on PLCSim on V14. I hope I can test this instructions on a physical CPU, but we haven't acquired one with FW 4.2 yet. |
"Engineers like to solve problems. If there are no problems handily available, they will create their own problems." (Scott Adams) |
|
This contribution was helpful to1 thankful Users |
Follow us on