10/23/2006 6:08 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating: (1438) |
Hi, look at the FAQ http://support.automation.siemens.com/WW/view/en/770453. It has a Error table with the possible solutions. In specital for Online problems with erro code 30:504 ther's the entry: " In this case the customer can check whether the MPI LED lights on the CP5611 during this time. - If the LED does not light, the module could be defective or there is an address conflict on the PCI bus (though unlikely). - If the LED lights, then there is an interrupt conflict. - NT Diagnostics ->Resources. - Warning: with some modules you have to switch the computer off/on after BIOS changes. A possible remedy could also be to plug the CP5611 into a different PCI slot. |
Denilson Pegaia |
|
10/25/2006 9:41 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello horatio, Pleas have a look at the following faq: http://support.automation.siemens.com/WW/view/en/17376617 When you 'upload' a programm, from CPU to PC, you lose the comments and symbols. Hope this helps. Best regards, Wizard |
7/10/2017 2:40 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by AutoGen_665942 is split to a separate thread with the subject Opening DB10: Error message 30:504. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on