1/9/2018 10:13 AM | |
Joined: 10/11/2017 Last visit: 3/21/2022 Posts: 32 Rating: (1) |
The/A solution to the problem was given in the next topic: With that there is no need for extra function blocks. TlDc: By selecting "Diagnostic Interrupt" in the CPU and enabling the "Value Status" on an I/O module an extra byte is set. You will then have 1 byte giving you the I/O status of the 8 channels, and 1 byte giving you the error status of the channels with 0 = fault and 1 = functional. |
Last edited by: Fichie at: 1/9/2018 10:15:01 AMLast edited by: Fichie at: 1/9/2018 5:17:21 PMLast edited by: Fichie at: 1/9/2018 5:17:41 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on