2/1/2018 10:59 AM | |
Joined: 3/26/2009 Last visit: 7/14/2024 Posts: 138 Rating: (0) |
TIA13 SP1. PLC 1215 and distributed profinet IO ET200M (6ES7153-4AA01-0XB0) I downloaded IO ET200M configuration, but TIA does not recognize the configured interface module. The diagnostic bufer message is: "Not reacheble. Difference between the loaded configuration and the offline project. Online arcticle number: "?" Offline article number: 6ES7 153-4AA01-0XB0. What error can there be? What difference can there be in the online and offline configurations if I just downloaded it from the project? How can this be fix? |
Follow us on