4/3/2018 5:06 PM | |
Joined: 7/7/2010 Last visit: 10/16/2024 Posts: 15319 Rating: (2432)
|
When the PS was not working, the PLC was the only device powering the backplane. It runs out of right where you noticed. Depending on the position of the PS in the backplane, it can add to the PLC or be the sole source of power to the backplane. In position 0 (left of the PLC), it adds to the PLC. I recommend that. If you used the TIA Selection Tool before ordering or placing components, you may have already seen the limits of just the plc by itself providing power to the backplane.
|
science guy |
|
This contribution was helpful to1 thankful Users |
4/4/2018 7:30 AM | |
Joined: 5/31/2017 Last visit: 6/21/2023 Posts: 5 Rating: (0) |
|
Follow us on