2/20/2018 5:27 PM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, the string: 16#@1%X@ serves as a placement holder which is filled with the data from one of the blocks. The @ charts are generated by the system automatically which provide diagnostics from the hardware. You wont't need to do anything in those blocks, it provides an interconnection between hardware and CFC user program
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on