5/6/2018 3:14 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear user, The easiest way is to provide a "RESET" input in the FB and initialize (False or 0) all critical or necessary variables.You can assign a global memory to RESET signal or use the IDB address and set this signal in OB100(OB100X). To bring the operation of FB into normal, you can wait for operators' intervention or do it automatically in your program(RESET=0 in OB1 or OB3X). Check the attached file as a sample. I hope it helps, hdhosseini AttachmentPID_GENERIC.txt (66 Downloads) |
Last edited by: hdhosseini at: 5/6/2018 3:21:26 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on