8/14/2018 12:46 AM | |
Posts: 39 Rating: (0) |
Unable to do that even though the CPU is in STOP mode The action cannot be performed in the current operating mode of the module.,8/13/2018,3:45:11 PM |
8/14/2018 1:38 AM | |
Posts: 39 Rating: (0) |
It seems like if I recreate the project from scratch in TIA V14 instead of migrating everything works fine, and I am able to download without problems. |
Follow us on