5/31/2013 6:27 AM | |
Posts: 4 Rating: (0) |
Hello everyone, I have almost the same issue. I have Windows Xp Sp3, Step 7 5.5 and i have a s7-414h blank from factory. So i need to download the first HW Config via MPI and then work via Industrial Ethernet. However i have no connection and keeps telling me to check cabling or media. im using PC Adapter 6ES7-0cb20-0xa0 v1.2 from my engineering station to the PLC directly with no results. As a second option i have a windows Xp Sp2 virtual machine where i started to develop my program and runs under Windows 7. Using a virtual machine affects the behavior of the PC ADAPTER? In my PC adapter i have MPI, POWER, USB leds lit and i have no idea why Auto test is not working in PG/PC interface. This thing is driving me crazy. PC MPI ADDR = 0 DEFAULT PLC ADDR = 2 MPI DEFAULT SPEED 18x.5 kbps ( i dont remember it exactly) any ideas? Probably my PC ADAPTER is ruined :p thnx in advance. |
Last edited by: O_Moderator at: 5/31/2013 11:21 AMnew subject after splitting from /tf/WW/en/Posts/57995#top |
|
Follow us on