5/2/2020 5:28 PM | |
Joined: 3/11/2015 Last visit: 6/25/2024 Posts: 68 Rating: (1) |
Hello, I have a similar issue, due to some SQL error due to which couldn't open the SQL by connecting to its server, so my colleague had reinstalled it but now couldn't find the SQL WinCC server, only could find default MSSQL Server and i have configured in my project for SQL WInCC. SQL 2014 is used. WinCC RT Advanced V14.0 is used And my question is how to get that SQL Server WinCC ? Kindly let me know. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/04/2020 10:57:48New subject after splitting |
|
5/7/2020 10:11 AM | |
Joined: 8/3/2009 Last visit: 8/7/2024 Posts: 13468 Rating: (1704)
|
Hello Its not clear whats your problem... Do you want to connect to the SQL Server in the WinCC Advanced Runtime for Archives or in VB Script (LINK)? If this case this works with an ODBC Connection that you have to create in the Windows Settings first. The WinCC Advanced RT has no SQL Server instance or Installation by itself. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on