6/19/2020 12:57 PM | |
Joined: 8/3/2009 Last visit: 10/14/2024 Posts: 13919 Rating: (1757)
|
Hello It sounds a little bit like DPI : https://support.industry.siemens.com/cs/ww/en/view/13899072 -> Set your PC to 100%-> 96 DPI-> then do a compile of the Panels SW with rebuild all and do the test again then it should look like you need. If this is not the reason the nplease post a few screenshots of te behaviour. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on