6/26/2020 10:18 PM | |
Joined: 2/1/2010 Last visit: 7/12/2024 Posts: 148 Rating:
|
Hi vadrad, Between steps 3 and 4 are you sure you can go online with the project? Are you sure there is nobody else making downloads to the AS using a different ES with the original project between steps 4 and 6? Or that you accidentally made a download during your 'offline testing'? Otherwise this is not supposed to happen as long as you have not downloaded your AS after step 4 archiving the running project which matches. Archives are pretty much transferable indefinitely as long as the last download timestamps match. I've restored an archive after multiple years later, on different machines, etc and it always works unless there was another download which was not archived. In your case the my expectation is the STOP download reason are just that the project is somehow not of the same 'lineage' due to intermediate download. If the AS experiences a download which happened after your last archive and you need to revert to the configuration you will always have a STOP download if you restore an old project which has a download timestamp older than the AS. All the other rules about STOP downloads are published pretty well in the manuals, including all the rules around tCiR etc. Sorry I don't have a link handy ATM. |
If my post helped you, please rate. Thanks. |
|
6/27/2020 10:18 AM | |
Joined: 9/9/2015 Last visit: 6/24/2024 Posts: 727 Rating:
|
Dear vadrad, Can you do the following 1. After the CPU went to Stop unintentionally -> Do nothing and 2. Then go to CPU module information (online) 3. Look for "Stack" 4. Take a picture and try to understand the diagnostic info. 5. You may share it to us as a screenshot here. Hope this helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on