9/3/2020 2:53 PM | |
Joined: 7/5/2013 Last visit: 10/2/2024 Posts: 3114 Rating: (512) |
Hello algorithm, please have a look in the following FAQ: Tips and tricks for creating scripts in WinCC (TIA Portal)
Regards, Frink |
Pi is exactly three! |
|
9/3/2020 6:58 PM | |
Joined: 12/20/2013 Last visit: 10/1/2024 Posts: 46 Rating: (1) |
Hello Frink, Thanks for the link very interesting! However it appears that the issue is not related to triggering the script but to the detection of the event itself because as I explained I tried to set a value by the event but didn't work also. I believe that only the change of value for bool works for RT Advanced! Detection of exceeding/falling event maybe works with RT Professional! Would appreciate to know if anybody detected the exceeding/falling event to trigger any action whatsoever while running RT Advanced! Algoritm |
Follow us on