6/8/2015 2:29 PM | |
Joined: 1/28/2009 Last visit: 7/11/2024 Posts: 6844 Rating:
|
Hello, To configure 6ES7314-6EH04-0AB0 , you need STEP7 V5.5 or higher with HSP191 as a conventional way.It is also possible to use the following GSD file for a DP slave configuration in a given configuration editor. Station type: CPU 314C-2 PN/DP V3 I hope this helps, hdhosseini |
This contribution was helpful to
1 thankful Users |
6/8/2015 2:32 PM | |||||||||
Joined: 9/27/2006 Last visit: 7/13/2024 Posts: 12268 Rating:
|
Hello Anshuman;
As you can see from the extract above, you need at least Step 7 5.5 with a HSP (hardware service pack, not a gsd) to insert the new CPU in your hardware ccatalog.
See the following information, where the table above was taken:
New S7-300 Compact CPU 314C-2 PN/DP Released for Delivery Hope this helps, Daniel Chartier |
||||||||
This contribution was helpful to
1 thankful Users |
Follow us on