11/27/2020 9:07 PM | |
Joined: 3/14/2008 Last visit: 8/13/2024 Posts: 2084 Rating:
|
Hi, You could send the elapsed value to a MonAnL block for example. If you make the block IO: "EN" visible, you can use that to freeze the value of the block. If "EN" is set to 0, the block is not executed and the elapsed time is shown at the output: "Out" and not changing anymore until you set "EN" to 1. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on