3/20/2019 11:03 PM | |
Joined: 1/4/2013 Last visit: 7/12/2024 Posts: 1117 Rating:
|
Hello Master. I retried everything and these are my results (see attached file) 1) I downloaded the GSD file of et200SP 2) I opened TIA without opening any project and I started installation of that GSD 3) After like 25 minutes of 0% in the task bar, the percentage ran at 1%, then 2%, then ... 100%, until I got the installation complete message, without any errors. 4) I closed TIA and reopened it, and I opened my project. 5) I tried to insert that ET200SP, of course I searched in "other field devices" (in italian is my TIA V13.1) but I only see the IM151-3 (which are ET200S), but no ET 200 SP or equivalent SIemens code. (See attached file). 6) I wanted to be more frustrated than this: I opened again the tool to install the GSD , I selected the GSD I have installed before and it says that ... "it is not yet installed"... Like I have never done this procedure... Sigh, Chris, what I can do ? I don't want to populate the world every year with 100 machines with "red leds for nothing"... AttachmentScreens.zip (154 Downloads) |
Last edited by: Davinator at: 3/20/2019 11:04:11 PMLast edited by: Davinator at: 3/20/2019 11:04:56 PMLast edited by: Davinator at: 3/20/2019 11:05:52 PMLast edited by: Davinator at: 3/20/2019 11:07:08 PM(Sorry for the zip but I cannot load multiple attachments) Searching for Siemens used/new equipments ? |
|
3/21/2019 11:25 AM | |
Joined: 5/12/2006 Last visit: 7/15/2024 Posts: 22312 Rating:
|
Hello, for V13 SP1 the latest UPD is 9 https://support.industry.siemens.com/cs/ww/en/view/109311724 you must not update Scout TIA, only the TIA Portal.
Christoph |
3/21/2019 10:37 PM | |
Joined: 1/4/2013 Last visit: 7/12/2024 Posts: 1117 Rating:
|
Hello Master, I have installed the TIA 13.1 Update 9, as you suggested. Unfortunately the result is the same. Upd 9 was succesfully installed, rebooted the PC and installed the GSDML of the ET200SP. Installation took like 30 minutes and I got the same results of when I had the upd 6 installed, so installation is successful, but if I look at the GSD it says "not yet installed", and of course the hardware is not present in the devices list (other field devices in english, but w/e).... What I can do ? Can you make me a SS of your tia 13 hw catalog where I see that ET200SP ? Just I am curious of how it would appear... Attached there is the ss of what I have done... Danke in advance
|
Searching for Siemens used/new equipments ? |
|
3/22/2019 6:06 AM | |
Joined: 5/12/2006 Last visit: 7/15/2024 Posts: 22312 Rating:
|
here the ss from my system |
This contribution was helpful to
1 thankful Users |
Follow us on