9/5/2019 3:48 PM | |
Joined: 8/21/2019 Last visit: 12/16/2022 Posts: 7 Rating: (0) |
The project transferred from WinCC 2008 SP2 to Tia portal v14 comfort sp1, then to Tia portal v15. 241 errors occurred while compiling. As a guide, I deleted the old S7-200 connection, but did not find S7-200 in the catalog. What to do? I attach the project archive.
AttachmentWinCC_flexible_2008_SP2_tmp44_V15.zip (225 Downloads) |
9/5/2019 4:00 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
Errors appear because HMI Tags are not connected to real data. - In the Connections editor, create a connection to the S7-200. Communication driver - SIMATIC S7-200, set the connection settings. - In the HMI Tags editor, set the Connection property to all external tags. AttachmentScreens.zip (245 Downloads) |
This contribution was helpful to1 thankful Users |
9/11/2019 1:30 PM | |
Joined: 8/21/2019 Last visit: 12/16/2022 Posts: 7 Rating: (0) |
Thank you very much! It seems that everything worked out. It is also necessary to check on the installation. |
Follow us on