9/10/2015 10:12 AM | |
Posts: 26 Rating: (0) |
Hi ChristophD, Yes, we are talking about motor_7, please find the screenshot in the attachment. and I also have another errors, not just the Fault 1482. In the attachment you can see the errors just before i switch on the sistem. Also if I run the machine, it runs for a couple of seconds, and then D445 goes to stop mode. errors are in the next post. Thanks, AttachmentErrors_After Switch on.pdf (152 Downloads) |
9/10/2015 10:12 AM | |
Posts: 26 Rating: (0) |
Errors after Run...
AttachmentErrors after run.pdf (166 Downloads) |
9/10/2015 12:36 PM | |
Posts: 26 Rating: (0) |
I think is this one, |
9/10/2015 12:40 PM | |
Posts: 1529 Rating: (202) |
looks like either 05 or 06. Need some more information on these. |
Follow us on