4/26/2016 12:23 PM | |
Joined: 8/14/2014 Last visit: 4/5/2024 Posts: 144 Rating: (17) |
I think it's standard for power suppliers to deliver energy with different prices for different day peroids? |
4/26/2016 12:52 PM | |
Posts: 21 Rating: (0) |
how ? can you give me the steps ? thank you. |
4/26/2016 2:14 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello We had a similar requirement from a customer, so we calculated the energy consumption in Various Tariff periods and Tariff in a PLC and Generated reports in WInCC. The Tariff timings and stored in a DB can be selected based on Date & Time. However if your budget permits, the following EMS softwares have similar features . Pl see if they suit you : SIMATIC Power Control SIMATIC B.Data Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
4/26/2016 4:18 PM | |
Posts: 21 Rating: (0) |
So what i should do to success to do it ? |
4/27/2016 4:14 PM | |
Posts: 21 Rating: (0) |
is that the format of the configuration is like this? (it's an example) |