11/10/2014 6:22 PM | |
Posts: 21 Rating: (0) |
Hello, could anyone give me advice where can be fault? I have interconnected CPU (6ES7214-1AG40-0XB0) + HMI (6AV2123-2GB03-0AX0) + NTB. The connections are through switch. IP addresses are 192.168.0.1-3 on the devices. Other setting of devices are more or less defaults. When are CPU+HMI connected (NTB is disconnected from switch), no error is on the CPU. When the NTB is connected to switch the error on the CPU appears and blinking. But I can download sw to HMI even CPU without faults. Do you have an ideas where can be problem? I have attached the diagnostic file from TIA. Thank you very much for advices! Ales AttachmentDiagnostics.pdf (147 Downloads) |
11/11/2014 8:33 AM | |
Posts: 1368 Rating: (126) |
Can you please give more informations about hardware, hardware topology (screen from TIA), given IP, TIA Version... Thanks! |
11/11/2014 9:01 AM | |
Posts: 21 Rating: (0) |
HMI screen |
11/11/2014 10:14 AM | |
Posts: 21 Rating: (0) |
wrong partner HW_ID 65 probably is connected NTB (notebook) switch hasnt speciffic configuration. It is basic simple switch. NTB- I mean notebook ! |
11/11/2014 10:15 AM | |
Posts: 21 Rating: (0) |
event 1 |
11/11/2014 10:15 AM | |
Posts: 21 Rating: (0) |
event2 |
Follow us on