12/11/2023 5:58 PM | |
Joined: 5/15/2023 Last visit: 12/26/2023 Posts: 19 Rating:
|
Hello. Wipotec uses the CAN protocol. I use Wago 750-375 and Wago 750-658, initially it was in a working machine. The car is broken, but the spare parts remain The example I gave shows how communication with the Siemens CAN module is carried out, it is well shown how the engineer configures the device to work with the CAN interface, downloads EDS files. When I try to set up the Wago 750-658 hardware, it is not possible to download the EDS file, so I cannot specify registers, addresses, and PDOs. I don't understand how I can set up the hardware to work. Please see picture Attachmentcan.zip (212 Downloads) |
Last edited by: master_138 at: 12/11/2023 18:01:04Last edited by: master_138 at: 12/11/2023 18:02:08Last edited by: The Helping Hand at: 12/12/2023 09:20:24Text formatting optimized |
|
Follow us on