8/16/2018 7:46 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear All, It's mentioned everywhere that only "runtime relevant" portion of code is loaded from load memory into work memory of a PLC. It's also clear, that one can clearily see the occupied size in load memory and code-work memory AFTER the program is written. But is there any way to estimate load-memory size and "runtime-relevant" memory size of a program BEFORE the program is written? Because it's more common, that the CPU must be selected and purchased before the program is ready, and even before the program is started being developed ) Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: _Pavel_ at: 8/16/2018 7:46:48 PMLast edited by: Jen_Moderator at: 8/17/2018 7:25:37 AMNew subject after splitting |
|