1/10/2012 1:20 PM | |
Posts: 66 Rating: (0) |
I changed it in to 5 but there is still a maximum off 5 connections in the CP yours, J. Timmermans
|
1/10/2012 1:31 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
http://support.automation.siemens.com/WW/view/en/23369901 |
1/10/2012 1:40 PM | |
Joined: 9/28/2005 Last visit: 7/10/2024 Posts: 2957 Rating: (242) |
As I understand from responses this trick is not helping. |
Best regards, |
|
1/10/2012 4:25 PM | |
Posts: 66 Rating: (0) |
Could this be a isue? Please see attachement yours J Timmermans
AttachmentCyclic operation.pdf (65 Downloads) |
1/10/2012 4:42 PM | |
Posts: 66 Rating: (0) |
see firmware in attachement. There is no newer version then V2.2 for the HW configuration. yours, J Timmermans
Attachmentfirmware Lean.pdf (91 Downloads) |
1/11/2012 8:08 AM | |
Joined: 9/28/2005 Last visit: 7/10/2024 Posts: 2957 Rating: (242) |
Hi timmermans Maybe this could be very good idea to post issue to the Siemens Support ? They should explain the issue about 5 connections instead of 4. And post answer here. Its very interesting. |
Best regards, |
|
Follow us on