4/7/2018 8:47 PM | |
Joined: 12/7/2011 Last visit: 6/21/2024 Posts: 384 Rating:
|
Hi to all, Taking a cue from the "Template from a new topic post" I start providing the system details im using: - Win 7 Pro sp1 x64 - Tia Portal V13 SP1 upd8 - Rack 1; S7 315-2 DP and CP 343-1 Lean - Rack 2; IM 153-2, AI nad AO. Im pretty confident with the Step7 (up the 5.5 version) but not so much with tia portal, this means that i know how work the Siemens' IO addressing. So, once completed the hw configuration, and put in running the cpu, i get the "Area length error when reading" error, and i knows very well this error occur, and i've already checked many times the hw configuration, and seems to be ok, but for some reasone, im still getting the error. I've attached the hw configuration, i kindly ask to verify if i miss something. Thanks to all. Ragards. Duccio. AttachmentHW Tia portal.pdf (180 Downloads) |
Follow us on