(0)| 3/16/2021 1:04 PM | |
|
Posts: 16 Rating:
|
Hi All! PCS7 8.1 - OS Server with redundancy - Win Server 2008 R2 Standard UPD: Servers and clients are using VNC Server V5.1 since at least 2 years. After the failure i have to do a complete download. The complete download does not present any problem at all. Here you have the log returned by Simatic Manager: Load Online Changes;Could not establish connection to the computer 'OSSERVER02'. Load Online Changes;Loading online changes to "OSSERVER02" has been stopped because the connection was terminated. Load Online Changes;Execute a download of the entire program for the server. Load log ================================================================================ Source: E:\PROYECTO\Ecoparc1\Hmi\wincproj\OSSERVER01\winccom\ Target: \\OSSERVER01\PROY\OSSERVER01\OSSERVER01.mcp Project type: Master MAKE: No Date: Friday, March 12, 2021 07:53:38 Display load log... ------------------- 12/03/2021 7:54:05 : Only the configured changes will be transferred to the runtime OS. 12/03/2021 7:54:17 : The project was opened successfully. 12/03/2021 7:54:28 : The Picture Tree was updated in 00:00:11. 12/03/2021 7:54:42 : Server data were created successfully. 12/03/2021 7:54:42 : The download of the Standby OS is started. 12/03/2021 7:55:12 : Cancel: Load Online Changes: Could not establish connection to the computer 'OSSERVER02'. 12/03/2021 7:55:12 : Cancel: Load Online Changes: Loading online changes to "OSSERVER02" has been stopped because the connection was terminated. 12/03/2021 7:55:12 : Cancel: Load Online Changes: Execute a download of the entire program for the server. 12/03/2021 7:56:05 : Cancel: Standby OS could not be loaded: 12/03/2021 7:56:05 : Error no especificado. Return value: 800040050X 12/03/2021 7:56:19 : Caution: Loading online changes failed. Duration: 00:02:13. 12/03/2021 7:56:19 : Cancel: An error occurred while downloading to the target system. UPD: There is an Application Event on the attached ZIP Thank you all for your time!! AttachmentRepeticion error al descargar slo cambios Server02.zip (277 Downloads) |
Last edited by: Fedena2507 at: 03/17/2021 09:29:50Last edited by: Fedena2507 at: 03/17/2021 09:56:14 |
|
| 3/17/2021 7:56 AM | |
|
Posts: 7298 Rating:
|
Hello Fedena2507, the HResult 800040050X is an "unknown" error. Had you used the RDP (Remote Desktop Protocol) to access the see FAQ: https://support.industry.siemens.com/cs/ww/en/view/78463889 Regards Georg Berghof |
This contribution was helpful to
|
|
Follow us on