Default Header
(header konnte nicht geladen werden)
(0)| 4/7/2021 2:54 PM | |
|
Joined: 12/18/2014 Last visit: 1/22/2026 Posts: 36505 Rating:
|
At the digital inputs of a 230 LOGO! signals with 5 VDC cannot be evaluated. The switching thresholds for recognizing a LOW or HIGH signal are higher (see appendix). And the 230 LOGO! has no analog inputs. If you want to evaluate 5 VDC with an analog input, you need the analog extension module AM2.
AttachmentLOGO! 8 manual 0BA8 2014_06 page 294.pdf (552 Downloads) |
Last edited by: ixo65 at: 04/07/2021 15:08:37Attachment |
|
Follow us on