11/20/2007 9:51 AM | |
Posts: 2930 Rating:
|
Hi, Over Ethernet you have to configure additional communication parameters for PC-Access. Follow the steps in this desciption it should work. Regards Helmut AttachmentTSAP PC-Access.zip (628 Downloads) |
11/23/2007 9:23 AM | |
Posts: 20 Rating:
|
Thank You very much now i m able to communicate Regards, Sudha.. |
2/21/2009 8:25 PM | |
Posts: 19 Rating:
|
Matthias See my thread Is TSAP hard to understand? under Communication / Networks from today. If you still has problem send me a private message and I try to help you out. I dont believe I'm an *** but it took me weeks to understand it enough to set up the six channels I needed betweenthree 224XP and the PLCs to PC-Access. You also need a strong TCP/IP network as if you configure wrong your network goes flat! Dan |
Follow us on