(0)| 8/12/2021 1:14 PM | |
|
Posts: 61 Rating:
|
Dear Sir, May I know what is the IR_ready used for? It is a linking file or pusher application between WinCC and SQL server? Recently, I get the windows information log about this file is failed. ” failed to open the explicitly specified database "is ready". [ client: <local machine>] “ byI already reboot the server, but this log is continuously happen ------------------------------------------------------------------------------------------ |
Last edited by: WY. at: 08/12/2021 13:15:20Last edited by: WY. at: 08/12/2021 13:16:52Last edited by: Jen_Moderator at: 08/12/2021 13:50:02New subject after splitting |
|
| 8/12/2021 2:53 PM | |
|
Posts: 7298 Rating:
|
Hello WY., the WinCC stations and the PCS 7 Operator Stations (OS) need the "Information Server Ready" And the "IS-Ready"-database is a part of this component, "Information Server 2014 SP3" https://support.industry.siemens.com/cs/ww/en/view/109752435/104398144651
Georg Berghof |
| 8/13/2021 10:51 AM | |
|
Posts: 61 Rating:
|
Thanks your information. Attached the SQL Server A manager capture. I found the "IS_READY" is missing and the windows system also logged with:
As comparing with my Server B, the "IS_Ready" is existed and without the TWO However, should I add back the "IS_Ready" to the Server A? Should I handle the others TWO SQL file in the capture? How is the procedure to do this and need stop the WinCC Runtime? |
Follow us on