(0)| 9/21/2021 4:25 PM | |
|
Posts: 7 Rating:
|
Hi we would like to retrieve the WINCC alarm and events message. The software is PCS7 V7,1 SP2. I was told to use the Connectivity Pack 1. Make WINCC station as OPC UA server 2. Connectivity Pack will allow WINCC to store the alarms to external database server Also there is another package called Industrial Data Bridge. We would like to use our OPC client app to retrieve the alarm and event message already defined on the WINCC. Are the Connectivity Pack or Data Bridge the correct solution or any other suggestion? It will be very much appreciated if you can give some advice and the links to the documents to help us to make a correct decision. Thanks John ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/22/2021 08:10:19New subject after splitting |
|
| 9/22/2021 1:08 PM | |
|
Posts: 7298 Rating:
|
Hello AutoGen_403372, PCS7 V7.1 SP2 is an old version, it contains WinCC V7.0 SP2. see manual: https://support.industry.siemens.com/cs/de/en/view/109762744/7310749835
Georg Berghof |
This contribution was helpful to
|
|
Follow us on