(0)| 11/3/2021 11:34 PM | |
|
Joined: 2/17/2020 Last visit: 1/19/2026 Posts: 1251 Rating:
|
hi Mark! I don't know to what extent the script may be affecting the client's communication with the server, but I would recommend you check a number of things: - Is the WinCC server accessed via RDP? If so, I recommend you remove remote access and follow this FAQ. - Have you tried to delete the DCF file? I would try following this FAQ to eliminate possible inconsistencies. - Is the project SQL database configured correctly? This could affect the operation -> FAQ (even if it refers to PCS7, it also applies to WinCC without PCS7 installations). I hope some of this helps! |
|
A rating will be well appreciated. |
|
| 11/4/2021 11:42 AM | |
|
Posts: 7298 Rating:
|
Hello Mark!, The error message: means, there is a wrong C-script in Global Action, In most cases such access violations are caused by wrong handling see FAQ: https://support.industry.siemens.com/cs/ww/en/view/7929092
Georg Berghof |
Follow us on