(0)| 3/1/2022 5:20 PM | |
|
Posts: 42 Rating:
|
Hello All , I am using WINCC 7.4 . In my project i want to display message on screen . We are displaying this message with the help of text list. Message consist of Two part Static and dynamic . Example - " Valve XV1001 is open " Here XV1001 is dynamic (For other message device name can be different like XV1002) . Rest other text is static which is in wincc text list . Can anyone please tell me how to add dynamic string in this message ? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/02/2022 09:38:13New subject after splitting |
|
| 3/3/2022 3:32 PM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello which control do you use? if you use the Text list control then you can only display the test list itself. If you want to add dynamic text the you an also use the Combo Box control and a Script for filling: here a little video that shows: LINK Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on