Default Header
(header konnte nicht geladen werden)
8/8/2022 5:14 PM | |
Joined: 10/25/2021 Last visit: 5/21/2025 Posts: 5 Rating:
|
Hi everyone. I need to read the Fault Code of a SoftStarter 3RW55 using Profinet Interface. I've reached on SFC52 reading Data Set 92, that give to me several bytes do extract the info bit by bit as we can see on page 1 of the PDF attached (page 198 of "SIRIUS 3RW5 PROFINET communication modules"). But, I need to read that information in an interger value to connect this value to a fault list on Step 7. I've got the info readed by an interger value like showed on page 2 of attachment (page 168 of "SIRIUS 3RW50 soft starter 168 Manual, 09/2019, A5E35628455002A/RS-AA/001"). That is my doubt: How could I read the fault list information of a 3RW55 as an interger value??
AttachmentHelp Read 3RW55 Fault Code.pdf (672 Downloads) |
Follow us on