(1)| 10/18/2022 7:49 AM | |
|
Joined: 5/6/2022 Last visit: 1/22/2026 Posts: 589 Rating:
|
Hi Alain-J! I have seen that you have already configured Imhost and it seems that you have everything set up correctly, but just in case, I recommend you to check the following FAQ where all the steps to enable it are explained: "What are the requirements for operating SIMATIC WinCC in a Windows network?" Also comment that it could be an RDP issue, by this I mean that you are not accessing via RDP or a remote access not released to the server because it would pull down the WinCC server services. Could you share screenshots of the OS versions of the two PCs. Also the exact software you are using (You should have the same software versions on all of them). Best regards! |
|
If this Information really helps, you could use the Rate function |
|
| 10/21/2022 11:04 AM | |
|
Joined: 8/3/2009 Last visit: 1/23/2026 Posts: 16661 Rating:
|
Hello Alain you should check all Stations wich this FAQ: https://support.industry.siemens.com/cs/de/en/view/868014 -> Important also the lmhosts files! A trick is also you can use each other as Multicast Proxy in Simatic Shell. this shold not be necessary in a local LAN segment but I had also a constellation in the past that works only like this. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on